****************************************************************************

       ADSP-TS101S Multiprocessor Project - C Code

Analog Devices, Inc.
DSP Division
Three Technology Way
P.O. Box 9106
Norwood, MA 02062

September 2002 - MKB

------------------------------------------------------------------------------------------------

This file refers to the switches used in the project contained in this directory.

Project options: 
================

Please refer to the VisualDSP++ release notes and the 
TS101S anomaly listing for full details of the following switch usage, 
operation and silicon revision requirements

Assembler/Compiler switches to be used in the assembler and 
compiler property pages' Additional Options fields

'-default-branch-np'	Required for TS101S Rev 0.1 silicon. 
						Use in BOTH compiler AND Assembler property 
						page 'Additional Options' field.

"-align-branch-lines'	Required for TS101S Rev 0.1 and 0.2 silicon". 
						Although a specific example may not contain a 
						"jump(P)", to keep generality the switch is 
						required for all silicon versions. Use only 
						in Assembler property page 'Additional Options'
						field.


If any example code projects are built/rebuilt for the above mentioned 
silicon revisions, these switches must be used. The same holds true for 
user created code sets.